|
Test files and Applications -
Boot Loaders -
Go to here for the latest version and
information.
LCD Test Code -
SerLCD v1.0 (Hex,
Asm,
C)
- This is the code that is loaded onto the 16F630 that is used with our Serial
LCD product. Very simple, very effective. It should serve as a good example of
how to interface to the HD44780 LCD driver chipset.
PIC-MT
LCD Test Code (Hex,
Asm,
C)
- Works with the PIC-MTC. Displays a message on the LCD Screen. The code
is easy to adapt, and works at 20MHz.
PIC-PG4D UART Test Code (ZIP)
- Works with the PIC-PG4D loaded with a 16F628. This code reads in user typed
commands and displays them. The LED alternates on/off for each character
received. Make sure you also look at the header files!
Blinkin -
Random reference to Robin Hood - Men in Tights
Use these programs as test HEX files as well as easy to understand C examples.
We use these exact hex files to load and test boards using the PG1, PG2C, PG3B,
and MCP.
You may need to right-click on the following links and select "Save Target
As..."
These files will drive all pins on the PIC high/low alternating every second
(designed for 20MHz operation). If you've get an LED hooked up correctly to any
pin, it should blink.
12F629 (Hex,
Asm,
C) - Works with the P8 boards and In-Circuit (chip in a bread board)
- uses 4MHz Internal OSC
12F675 (Hex,
Asm,
C) - Works with the P8 boards and In-Circuit
- uses 4MHz Internal OSC
16F676 (Hex,
Asm,
C) - Works with the P14 boards and In-Circuit
16F84A (Hex,
Asm,
C) - Works with the P18 boards, the PIC-PG4B, and In-Circuit
16F628 (Hex,
Asm,
C) - Works with the P18 boards, the PIC-IOA, the PIC-PG4B, and In-Circuit
16F873A (Hex,
Asm,
C) - Works with the P28 board, the PIC-MTA, and In-Circuit
16F877A (Hex,
Asm,
C) - Works with the P40 board and In-Circuit
18F1320 (Hex,
Asm,
C) -
Works with the P18 board and In-Circuit
18F252 (Hex,
Asm,
C) -
Works with the P28 board and In-Circuit
18F452 (Hex,
Asm,
C) -
Works with the P40 board and In-Circuit
|